Other Parts Discussed in Thread: UCC27211, UCC27212, UCC27212A-Q1, , CONTROLSUITE
what is the max amps from Vdd 12v in this design? Can it be directly connected to the 12v battery or should be regulated?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
what is the max amps from Vdd 12v in this design? Can it be directly connected to the 12v battery or should be regulated?
Hi Jeff, thank you for your input. I am sorry but my question was 12v current requirements for TIDA-00364 schematic (not only UCC27211 chip in it). Can you point me to the way to arrive to the actual answer to my question using the data you provided in datasheet?
Calculating a total for 3 driver chips from the driver datasheet would assume they all charge/discharge simultaneously (which is not so i know), another assumption would be that duty cycle for each driver is NO MORE than 50% (?) and switching frequency 100kHz . Yet assumption might not be right for this design as TI tested it switching PWM to 10 kHz (what was 12v current in this test?) and also I am not sure if it was assumed that 50% is the highest duty cycle for this design. Or is it easier just to make a rough estimate only based on the data for a single driver chip?
"it is quite long way to arrive from peak current to the power supply DC current requirement for the whole design board , which is my question in this post"
Hi Vlad,
Sorry for the delay, as Jeff mentioned, I was out of the office.
We discussed this internally, and here's what we calculated:
Gate power = Qg*Vg*fsw = 144 nC *12 * 10k = 17.28mW
There are five FETs in parallel, total low side switch gate power = 86.4 mW
Total high side switch gate power = 86.4 mW (Simplified calculation - not included bootstrap diode and MOSFET Vdson drop while charging bootstrap cap)
Peak gate current is supplied by bypass capacitors. Average VDD input current for driving gate load = 0.172 W/12 = 14.33 mA
Leakage in R7, 19, 31, 43, 56, 68, 79, 89, 91, 102 gate to source resistors= 12/2k = 6 mA (Top and bottom switches are complementary, leakage will take place either across R7, 19, 31, 43, 56 or R68, 79, 89, 91, 102 independent of duty cycle)
UCC27211 IDD operating current at 10kHZ @ 25C,(CL = 0pF) = 120uA (figure 4 datasheet)
Boot voltage operating current at 10 kHz @ 25C,(CL = 0pF) = 140uA (figure 5 datasheet)
Total current for one gate driver = 20.59 mA
Average current from 12V input for three gate drivers ~ 65 mA
It will also depend on the Qg of the FET selected by him and his PWM frequency
We also have PSPICE models for the UCC27211 and UCC27212, so you could use those along with your exact operating conditions to get a value for the current drawn from the 12V supply.
Let us know if you have any further questions about this TI Design.