Part Number: PMP4303
Dear All,
one of my customer interested in reference design PMP4303, we have certain queries as below - request you to clarify.
1.There are two transformers and one inductor used in design, can we get transformer(core, bobbin, winding informations) and inductor specifications, so we can check for local manufacturing here in INDIA.
2.In pmp4303 has LDO which gives 5V output , but we need 15V output, can we use 15V regulator at the secondary side of transformer to get it? Currently I/P voltage max of 5V LDO used is 13.5V which means transformer is giving O/P less than or equal to 13.5V, if I am going for 15V LDO, do I need to change transformer design in-order to provide more input voltage than o/p of 15V?
quick reply in this regards wll be very grateful.
Aravind.