This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352 with single MT47H64M16HR-25E DDR2 question ?



Hi

Currently we have a customized design and we use DDR2 (MT47H64M16HR-25E)  on the PCB

We see a strange behavior on the DDR2 that 

-------------------------------------------------------------

1. configure DDR2 (please see below settings)

2. Write data from 0x80000000 to 0x8000001F  with 0x5a5aa5a5

3. read back 0x80000000 ~ 0x8000001F 100times and will get  

80000000 = 5a5aa5a4 80000004 = 5a5aa5a4 80000008 = 5a5aa5a4 8000000c = 5a5aa5a4 80000010 = 5a5aa5a4 80000014 = 5a5aa5a4 80000018 = 5a5aa5a4 8000001c = 5a5aa5a4
80000000 = 5a5aa5a4 80000004 = 5a5aa5a5 80000008 = 5a5aa5a5 8000000c = 5a5aa5a5 80000010 = 5a5ba5a5 80000014 = 5a5ba5a5 80000018 = 5a5ba5a5 8000001c = 5a5ba5a5

-------------------------------------------------------------

You can see that the bit0 will change from 0->1 but I have no idea what could make this happen ? Do you guys ever encounter such question ?

Below is my settings of DDR2:

#define DDR2_EMIF_READ_LATENCY 0x5 /* disable Dynamic Power Down */

#define DDR2_EMIF_TIM1 0x0666B3D6
#define DDR2_EMIF_TIM2 0x143731DA
#define DDR2_EMIF_TIM3 0x00000347
#define DDR2_EMIF_SDCFG 0x58805232 /* 0x59805232 */
#define DDR2_EMIF_SDCFG2 0x08000000

#define DDR2_EMIF_SDREF 0x00004950
#define DDR2_DLL_LOCK_DIFF 0x4
#define DDR2_RATIO 0x80
#define DDR2_INVERT_CLKOUT 0x00
#define DDR2_RD_DQS 0x40
#define DDR2_WR_DQS 0x00
#define DDR2_PHY_WRLVL 0x00
#define DDR2_PHY_GATELVL 0x00
#define DDR2_PHY_WR_DATA 0x40
#define DDR2_PHY_FIFO_WE 0x6A
#define DDR2_PHY_RANK0_DELAY 0x1
#define DDR2_IOCTRL_VALUE 0x18B

and our trace length is 

DDR_CK Trace: 1.14903 (inch)

DDR_DQS Trace: 1.13877 (inc)

Appreciate if I could get feedback. Thanks a lot