Hi,
so i am new using the TLV320ADC2101 and it is working fine now without the miniDSP.
No i want to try to use do some DSP with PurePath.
My question is, if my setup is correct and if i understood the noise reduction block right.
1- Is the Block ADC3x01 2x the correct one? (There is also ADC3x01 4x as option)
2- What is the correct Input to use? (There is Dec1xln/Dec2ln/Dec4xln)
3- I want to set ADC at 96kHz and do an average and output frequency is 48kHz, so that i can reduce noise.
Can i do this on miniDSP. Will my setup work? Delay first sample and add it to second?
4- Noise reduction, so if i select low frequency at 100Hz and high frequency at 20kHz,
it means all values below the threshold that is in this frequency range will be attenuated right?
Edit: If i build and generate the code i get this error message:
"Failed to allocate miniDSP_A coef memory - insufficient resources
Coef memory conflicts have been detected.
Manually resolve the conflicts or use the automatic interface address reassignment tool in the Component Interface Overview dialog."