This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3221: TPA3221 Power supply recommendations

Part Number: TPA3221

Hey guys,

I'm building a 2x PBTL mono amplifiers for 8ohms speakers out of the TPA3221 and I've got a couple of questions for you fine folks out there:

  1. Given that I intend not to use the internal LDO of the TPA3221 and it being 240V mains powered, what power supply solution do you recommend?
  2. What operating voltage is optimal given that I want near maximum output power? 
  3. I'd like to use the LM1972 for digital volume control, do I need a buffer/pre-amplifiers between the attenuators and the power amplifiers?

Best regards,

Håkon H.