Other Parts Discussed in Thread: TPA3220,
Hello, i am thinking if i can connect the inputs of the TPA3255 without the op amp stage ensuring that the single-ended signal are converted into balanced connexion? Is it possible to only connect the single-ended connexion to one input channel (by putting a dc blocking capacitor on the input A pin and connect it directly to the main signal source, and the input B pin to a same value capacitor, (like 10uf) but to the tpa3255 ground), like it is commonly done on the TPA3116 ? If i would like to do this, it's to minimize cost and achieve a better sound quality.
Thanks for your response to come.