Other Parts Discussed in Thread: TLV320AIC3106
Hi,
I have a Texas TLV320AIC3104EVM board and am trying to connect the LINE2R input to RIGHT_LOP using the analog input bypass pathway as per section 10.4 of the datasheet.
So in the 'Bypass Paths' tab I select 'LINE2R - Bypass' which generates a message in the 'Command Buffer' tab :
w 30 6C 80
As I understand the data sheet correctly, this should result in the signal I put into MIC2R/LINE2R coming out at RIGHT_LOP.
But I get nothing out which I don't know why.
The other issue is the command sent down the I2C, hex 80 is sent to register 108 but the data sheet, page 74, says bit 7 is reserved and bit 6 should be set to enable LINE2R bypass.
Is the data sheet in error?
Any help would be appreciated.
Regards,