This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/LM49350: LM49350 codec register configuration

Part Number: LM49350

Tool/software: Linux

Hi  Sir,

LM49350 codex driver code kernel version is only support linux2.6.24(3.x), I'm currently using the kernel version linux 4.9.37.
If the driver code is unable to update the new linux kernel version, please help support register configuration. Thank you!
1.Can provide the codec chip initialization register code.
2.Codec chip docking master I2S interface is in recording mode, register configuration.
3.Codec chip docking BT PCM interface is in the intercom state (including codec to BT transfer data; BT to codec to transfer data, codec to send data to the speaker to play), register configuration.
4.Whether the codec chip has a register to view the received or sent audio data.