Other Parts Discussed in Thread: TPA2016D2
Hi team,
Question1
Datasheet commented describes below:
“The default values for the TPA2017D2 AGC function are given in Table 2. The default values can be changed at
the factory during production. Refer to the TI representative for assistance with different default value requests.”
Default value of gain is fixed at 6dB, what the range of gain we can change (e.g., 3-10db?)?
Customer required specific gain changes to 12dB or 18dB, is it possible? what's the lead time of changes?
Question2:
As alternative option, customer can find TPA2016D (gain programmable via I2C), based on datasheet, Efficiency vs Output power (fig.15 &16)
Shows RL=4ohm seems better efficiency, but since basically low impedance of output is better, so why 8ohm is better?
Is there any difference between TPA2017D vs TPA2016D expect I2C programmable?
Question3:
TPA2016D seems alternative option gain control instead of TPA2017D, is there any option?
Question4:
Customer want 18dB, TPA2017D if the efficiency is not significantly getting worse, how the higher gain value affects efficiency?
Best Regards,
ny