Dear Sirs,
My customer asked us about specification of Roc and Ioc(latched) for TPA3255
The TPA3255 data sheet has the following these descriptions.
Does Rocp here mean min value and max value?
In the data sheet, Ioc is also described as a typical value.
This is because Test Condition is described in min and max.
If this is correct, the min value of Rocp is 47kΩ and the maximum value is 64kΩ.
Is this correct?
If they are different, please tell me the min and max of Rocp and Ioc.
In addition, there is the following description at the bottom of the data sheet page 18.
OC_ADJ values outside specified value range for either CB3C or latched OC operation will result in minimum OC threshold.
In addition, there is the following description at the bottom of the data sheet.
OC_ADJ values outside specified value range for either CB3C or latched OC operation will result in minimum OC threshold.
This is understood to be the minimum OC threshold for values outside the range of 47kΩ to 64kΩ.
Is this correct?
Also I have one more question.
In Figure 27 on page 18 of the data sheet, Ioc appears to be a linear inversely proportional line to the change in Roc in the figure of OC_ADJ Resistor Value Example.
However, when I create a graph in Table 3 on page 19, it looks like a straight line.
Can this change be considered as a straight line (or linear approximation?) as shown in the data sheet?
Best Regards,
Y.Hasebe