Hello,
I use the driver in combination with a speaker which coil resistance is around 7 OHM.
To disconnect the driver from the speaker I use the shutdown mode of the device. Due
the device specification the output is set into HiZ mode. If I do a simulation then with
the speaker connected to noise at the speaker is very low (mean level < 1 pV) which
would be okay. But I'm not sure if this true in praxis. I'm not looking for the 1 pV, noise
level of 1 uV over frequency would be still okay. I want to avoid to use a switch between
the driver an the speaker to make sure that there is no signal at the speaker if there is
no input signal at the TPA6211 input.
Thank you, best regards
Jan