Dear Experts,
May I know that how to generate 1 250 MHZ 1.2V clock?
Xiaoliang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Experts,
May I know that how to generate 1 250 MHZ 1.2V clock?
Xiaoliang
You may consider CDCM61001, which can generate 250 MHz from 25 MHz crystal or external clock. 1.2 V single-ended output could be achieved using the 3.3 V LVCMOS output with external resistive attenuator circuit. The device is pin configurable.
Regards,
Alan
Hi Alan,
Could I use the LVPECL as the output driver. And terminate it using a 100 ohm resistor for CLKO and CLKOB. Then AC coupled to my chip (Common mode voltage equal s to 0.6 V)? If yes, since VOD have a 0.6 - 1.2 V differential swing, is it possible to let the swing equals to 1.2 V, thus the output could swing 0 - 1.2 V?
If not, based on your suggestion, will the attenuator affect the performance?
Thanks
Xiaoliang