Hi,
I have few queries regarding the operations of PGA and calibrations in ADS1218,
1) Does PGA is used only for maximizing the input resolution? say 40mV for PGA =1 and 70nV for PGA = 128. If it have any other purpose, please let me know.
2) I observe that the ADS1218 consume more current on initial startup and also while reading the flash pages. Could you please share the logic behind the same.
3) It is mentioned in the Datasheet that the maximum data output rate is 1 KHz, (PROGRAMMABLE DATA OUTPUT RATES UP TO 1kHz) at the first page under the Features. Does it means that the maximum speed of digital output from "DOUT" pin is 1 KHz?. If not what is the minimum and maximum frequency limit for digital communication with the ADS1218.
4) Does Selfcal/SelfGcal/SelfOcal works only for PGA = 1?
4.a)At selfcal, IC connects the analog pins to reference voltage which is going to be always 2.5/1.25, and do gain calibration. Thus the full scale positive value will now be mapped to 1.25/2.5V.
What if PGA = 128, where the positive full scale value is 19.531mV.
4.b) At PGA = 128, Is the maximum input differential voltage and output is 19.531mV ?
4 c) At what time we have to use selfcal and syscal (differentiate )
5) Does the differential input voltage should be always greater than or equal to 0V?. i.e we should not give negative voltage on any input channel (say, (-)1V or (-)2V on AIN0 )[Mentioned in ADS1218 datasheet pg.no 38 under table.5 as note(2)]
6) Is there any simulation tool available for testing this IC?
6) Relation between Fdata, Fmod and function of buffer in IC.
Thanks and Regards,
Makesh