I want to use the DAC part of AMC7836 to output -5V to 0V, so can I supply -5V to AVEE instead of -12V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I want to use the DAC part of AMC7836 to output -5V to 0V, so can I supply -5V to AVEE instead of -12V?
Hi Sarmad,
You can use a supply greater than -12V in this configuration. Note that the current sink capability when the output -5V will be limited if the supply is -5V. I recommend that you select a supply voltage that will provide some "headroom" when the DAC is at -5V. For that reason, I recommend you use a -5.5V or lower.
Thanks,
Paul