Sorry, that distract, I really tried to decide the problem myself.
I assembled the PCB board with ads1299 and start to measure the DC - voltage for checking (2 V). But the result was with noise. I decide to check the noise register - MUXn[2:0] - 00001001, and receive a very strange result,
16776020
16776019
16776019
it looks like the pin was connected to the reference, but in fact, should be to the ground.
bipolar power supply
I use the next setting for register (in fact I tried already many different settings for the register, but result in every time was the same)
ID - 0x3E
config1 - 0x96
config2 - 0xD1
config3 -0xE0
CH1SET - 0x09
MISC1 - 0x20
write_byte(CONFIG3, 0xE0);
write_byte(CONFIG1, 0x96);
write_byte(CONFIG2, 0xC0);
write_byte(0x04, 0x00);
write_byte(0x0D, 0xFF);
write_byte(0x0E, 0xFF);
write_byte(0x0F, 0x00);
write_byte(0x10, 0x00);
write_byte(0x11, 0x00);
write_byte(0x12, 0x00);
write_byte(0x13, 0x00);
write_byte(0x14, 0x0F);
write_byte(0x15, 0x00);
write_byte(0x16, 0x00);
write_byte(0x17, 0x00);