This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello E2E,
Since the Bit of the IC_Status register was 1 before writing the register value, the customer tried to clear the fault by writing 1 to CLR_FLT in the 0x4 register of DRV8316, but could not clear the Fault flag.
What is the reason why the Fault flag cannot be cleared?
Regrds,
ACGUY
Hello ACGUY,
Were all bits of this register "1", or only a few specific bits? If so, which ones? If so, that could indicate a persistent fault in the system.
Thanks,
Matt