Hello,
right now I'm trying to get one of the digital onboard microphones working on my AIC3263EVM-U Eval-Board.
In this first test I would like to route the signal of the digital mic to the headphone jack.
I'm using PurePath Studio and a sample rate of 48kHz with the following Setup.
I attached the project here:
7608.Test1.rar
Unfortunately I don't hear any sound from the microphone.
If I knock on the mic or the PCB it i get some signal but if i speak or whistle in it I don't hear any sound in the earpiece.
It seems like only the structural sound is received from the microphone.
Can anybody tell me what I'm doing wrong?
Do I have to configure the decimation filter in some kind?
Are there any examples how to use the digital mic with purepath or is it even possible to route it via Codec Control?
Thanks an lot in advance
Dennis