Hi everybody,
I am a little lost and need your help !
Here is the problem:
I need to use the embedded "Digital audio for record Path" of the codec (cf datasheet P.28).
Enabling the path is not a problem, as it is well described.
But what I want is to use this very function:
which is shown in the "TLV320AIC3104EVM and TLV320AIC3104EVM-PDK User's Guide", that you can find here:
http://www.ti.com/lit/sg/slau218a/slau218a.pdf
Actually it is a screenshot taken from the GUI software which allows to control the codec from a PC with the evaluation kit. My kit does not work anymore, I do not know why, tried to fix it but lost one day which is to much at this time.
It is a shame because I wanted to trace registers used in the log window available in this software to set the EQ filter.
So my question is simple:
As I can not find any "Gain", "Bandwidth" at "FC" fields int the registers shown in the datasheet matching this EQ register, is there a way to program it anyway ? I mean according to the picture above, if I want to set "gain = 3dB", "BW=300Hz" and "FC=1000Hz", what are the corresponding I²C packet to send ?
Thank you very much in advance for your help !!
F.