Hi,
with TLV320AIC3254EVM-K, I configured Audio Recording as Differential On-Board Microphone and if I try to record a wave file I have a DC component, as you see in the image.
There's a way to avoid this DC component?
Best Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
with TLV320AIC3254EVM-K, I configured Audio Recording as Differential On-Board Microphone and if I try to record a wave file I have a DC component, as you see in the image.
There's a way to avoid this DC component?
Best Regards.
Hi Mario,
Here is what I get with my EVM:
The offset is around -0.005 FFS.
I think I know what is going on. The descriptors of our previous USB audio firmware version (2.03) causes our USB controller to identify itself as a microphone. On Windows Vista onwards, this causes the OS to automatically add ~30dB of digital gain. This correlates to the fact that you are observing around -0.15 FFS of offset (0.005*30dB = 0.16 FFS).
We updated our USB firmware as a line input so that Windows will not perform this automatic gain boost. The latest f/w files can be found in http://www.ti.com/lit/zip/slac563. You can reflash the f/w by following the steps in 'AIC3254 CS > EEPROM Writer'. Once updated, I recommend you to uninstall the previous USB-miniEVM in Device Manager and reconnect the USB cable. It should then show up as a USB-AudioEVM in the AIC3254 CS main panel, version 3.04 (or newer).
If you run into any trouble, please refer to this wiki page: http://e2e.ti.com/support/data_converters/audio_converters/w/design_notes/2790.how-to-revive-an-aicdacadc-evm.aspx
Thanks,
J-
Hi J-,
I understand. Apart from the gain, in my application the offset is not negligible compared to the signal and this produce some issue on the post processing.
So I wonder whether there is a workaround available to remove this offset, hardware or software (miniDSP?).
We already developed a board with this codec and I absolutely need to remove the offset from the signal.
Best Regards,
mario
Mario,
You can do a high pass biquad filter in the miniDSP. Use the 'multi-biquad' component. This will remove any offset to 0.
Again, the offset you showed is not really the offset from the AIC3254 itself.
Regards,
J-
Hi J-,
thank you for the reply. I think that the IIR filtering is not a good idea for my application since the echo cancellation algorithm does not like this kind of processing. I could implement an HP-FIR or maybe it could be easier to apply an offset which removes the one introduced by the adc.
In any case, since I am working on a new design, I would like to understand if it is possible to remove this 0.005 FFS (more than 7 bit) with some design trick.
Thanks,
mario