Hi,
i'm trying to configure the PCM9211 so that it makes the following things:
- receive 3 type of input...one digital audio input connected to RXIN0; one optical input connected to RXIN2 and one I2S input connected to AUXIN1.
- i can select one of these input and drive it to the main output port.
- at the same time, the selected input will be drived to MPO0 through the DIT.
The problem is the following: if i select as source the RXIN2, in output i have both signals (a I2S from the main output port and a digital output in MPO0). If i select the AUXIN1 signals i have only the main port output, and nothing comes out from the MPO0.
The AUXIN1 signal is an I2S with 24bit RJF and a bit clock 64fs.
Below my simply configuration:
- 6Bh --> 44h (to select the AUXIN1 for the main output port)
- 60h --> 44h (to select the AUXIN1 for the DIT)
- 34h --> 02h (to select the RXIN2 as input for the DIR)
- 2Fh --> 00h (to configure the DIR as 24bit RJF)
- 61h --> 12h (to configure the DIT as 24bit RJF)
Let me know.
Silvio.