Dear Sir,
May I ask a question if PCM1863 Analog PGAs are enable and workimh when (2ch) differental Inut mode?
I refer to AK4620B. It enables PGAs at ony single end mode. When it set to differential, PGAs are disabled.
Then I wounder if PCM1863 has same issue. If the PGAs work without denpeding on analog input either differential or sine end, it will be great.
Best regards,
Masa