I recently purchased the PCM1865EVM. Surprisingly the datasheets are very incomplete with almost no mention of TDM mode interface of the device.
There are no descriptions on how this mode is supported, no timing diagrams either.
There are hundreds of registers to setup in order to make the device work but unfortunately no write ups or sample code details provided to make programming easy. After so many days of hardwork I could now get it to interface with my DSP but so far only in I2S mode. But I need it to work in TDM mode. But no info in the datasheets to setup the device properly in this mode.
The EVM is of very little use as it does not help generate/export the DSP coefficients data etc required to setup the device.
Hope some one in TI will address these issues.