Dear Support Team,
I have questions about PCM1802.
Our customer faces noise issue of it, and audio speaker sounds noise during no sound data(like a mute).
We want to improve it.
1.)
When VinL and VinR connect ground(like a mute situation), LSB 10bit data[9:0] of I2S is toggling(I2S 24bit mode).
We expect I2S data is zero(or more few toggling of I2S data such as only LSB 1bit), but I think this LSB data toggling is a little large for only PCM1802 noise.
Do you have any idea to improve it except Vcc, Vref?
If it is the spec of PCM1802, please let me know about it.
2.)
I2S data is 24bit and Vref is 2.5V(0.5 vcc).
In this condition, is following understanding correct?
I can't find the format of audio digital data in datasheet.
■PCM1802 Settings
SCKI :12.288MHz
LRCK(Sampling Freq):48kHz
BCK(Bit clock) : 64x48kHz = 3.072MHz
Interface mode : Master mode (MODE1=1, MODE0=1)
Format : I2S 24bit (FMT1=0, FMT0=1)
OSR : Oversampling ratio select=1, x128fs
BYPASS : Low (Normal mode)
Best Regards,
y.i