Hi, the PCM 1795 documentation says it supports up to 192KHz input and 8x Supersampling. Does that mean the internal sampling rate of the filter can perform at 1536KHz? Perhaps there is a lower ceiling such as 384KHz, and the level of supersampling will self adjust when this maximum is hit?