Hello all,
I have a TLV320AIC3254EVM-U. I have been using the included GUI to play around with it. It has been working great for a while, Then I tried to do a very simple digital in, analog out in PurePath. While downloading to the EVM, PurePath asked to change the sample rate. It changed it, and it has not worked since.
I did the EEPROM upgrade to V302 V304 more than 10 times, I even downgraded to V202. I uninstalled all of the windows drivers, and I even did a fresh install of windows. Still no luck. Windows detects the EVM, and it shows that it is outputting audio. When I use the included GUI, and load "Playback" you can hear a click of the DAC powering up. The GUI, talks to the EVM like there is nothing wrong. And if you load the spectrum analyzer, all the bars are maxed out. If you hook up to audio in, while audio is playing, you can hear a crackling sound in the headphones, but it is very low.
I just dont understand what is going on, and how changing the sample rate could brake my EVM. I want to get this working again, because I cant afford to buy another one.
PLEASE HELP,
Thank you
Anthony
*** EDITED *** I typed in wrong version number.