Hi,
I am trying to activate the EVM with digital mic.
I am using in the CS tool.
I managed to receive Analog mic with no problem.
When I am connecting the EVM to the PC, It sends data from PC to EVM IIS and then output to the headphones/speaker.
It is Playback in cs toold.
But when trying to connect digital mic - I have problems:
Connecting the mic data to Din
Connecting the mic clk to Scl (and to Bclk)
Connecting the mic L/R to Wclk
Configuring BCLK (Page0,Register27, bit3) and WCLK (Page0,Register27, bit2) as output.
Bclk is On (Page0,Register 30, bit0) and divider is set in the right divider.
And still nothing is getting out to the speaker
The maximum that I get is white noise.
How can I configure the AIC3254 for acquiring IIS mic data (and outputting it to speaker) ?