HI team,
I have a issue when help customer tuning EQ about PCM5242
Issue: Add an EQ at high frequency, scale voltage(reference voltage level) of all band will decrease a lot.
For example If adding an EQ (6dB Gain,Q=1.6)at 1kHz, output voltage at this point will increase about 6dB,and there is no effect to other frequency point,
But if adding an EQ(6dB Gain,Q=1.6) at 16Khz,output voltage will only increase about 3dB,and the scale voltage of all band will decrease.
This will cause if adding an EQ (Gain>0dB)at high frequency(16Khz), the output voltage at lower frequency(1Khz) will decrease.
How to solve this issue? Customer want to realize when adding an EQ at high frequency ,there is no effect to the scale (reference voltage level).
|
No EQ |
6dB Gain,Q=1.6 |
|
input signal is 1khz,0.125FFS |
0.9727V |
EQ frequency=1k Output voltage:1.93V |
|
input signal is 16khz,0.125FFS |
1.043V |
EQ frequency=16K Output voltage:1.541V |
|