Dear Tier.
My customer is going to design TAS2560 in her Audio System for IOT.
There are several qustions now
1. In my system configuration, I2S into TAS2560 come from AP(BCM). I cannot found Volume control registers in TAS2560 although datasheet describe all of mode configurations included volume block after ASI In stage. Currently I'm waiting for getting EVM from TI, I belive I can found how the volume block is operated in TADS2560. But could you let me know before I test EVM because I have to consider where I control volume process in the system, AP or TAS2560..
2. How many memory capacity for register setting of TAS2560 is requiered? Basically I'll leave the default setting after reset.
3. Is there any example code for below System Configuration?
1) MCLK : 12.288MHz
2) LRCK : 48KHz
3) I2S
Thanks / BR