Hi,
I use a PCM2707 in my design, with the SPI i'm able to send command like Play/Pause Next Previous so I think the hardware is OK.
I want to use the SPI to program the device descriptor to configure the Product and Vendor strings
I want to precise this is not a trouble of D+ pull up I desactivate it during the device descriptor programming.
I have noted the data should be sent from LSB to MSB and also they should be sent continuously after the ADDR bit has been set to 1.
I think this maybe coming of timing issue.
If we look to the page 24 of the datasheet I should be in the case continuous write operation to send the 456 bits of ROM
My question should I have a delay between each 16 Bits?
Do you see others explanations? or any advice ?
Thanks in advance
Best regards,
Matthieu