Other Parts Discussed in Thread: PCM5100
Hi Team,
Could you help review PCM5100A schematic?
Thanks,
SHH
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Scott,
I have reviewed the schematic section of the PCM5100. In general it seems fine, however I see an issue with the power of the device. When I/O voltage is 1.8V, DVDD and LDO pins should be connected to 1.8V power supply; in the schematic, LDO is not powered. The internal LDO is only functional when DVDD is 3.3V, offering the option of disabling it by providing a 1.8V supply to LDO pin for low power operations. So, please recommend customer to connect 1.8V supply to LDO pin.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer