Hi,
I would like to ask you some basic questions about the ADC reslution as below.
1) There are some kinds of resolution about ADC.
For example, about ADS1232, there are 3 resolutions --- Resolution(No missing code), ENOB(Effective number of bits) and NFB(Noise Free bits).
I do not understand well the correct resolution of the ADS1232 and I do not understand well the use case of ENOB and NFB.
Could you teach me how to use both specs, ENOB and NFB?
Normally should I use NFB as the true resolution of the ADC??
2) Resolution vs Sampling rate and PGA gain
The NFB and ENOB values are decreased(=worse) as sampling rate and PGA are increased.
About the sampling rate, I suppose that probably like internal switching noise is increased as sampling rate is increased.
So the noise will influence the resolution.
But about PGA, I do not understand well why the larger PGA is, the smaller the internal noise is?
(ADS1232 datasheet, P5, table 1 ~ 4)
I suppose that the internal noise of ADC is not changed by PGA gain...What is my misunderstanding?
I'm sorry for my poor questions.