Hello,
I am trying for the first time to run an ADS131E04 as a stand alone ADC. DRDY signal has a frequency of about 32 kHz. By watching DRDY with the scope I was able to find out as follows:
- RESET (06h) stops DRDY
- START (08h) starts/restarts DRDY
- STOP (0Ah) stops DRDY
- SDATAC (11h) doesn't stop DRDY!
I guess as I am not able to stop Data Continuously mode, cannot write or read out any register.
I am using Power-up timing like in Page 27(Figure 23) and start-up sequencing like in page 33 (Figure 31). I will appreciate any tip or help in this direction.
Regards,
Flori