Hi,
I'm looking for a 10-bit DAC that can support 8+ devices on a single bus. The analog outputs must be isolated from each other, so a multi-channel device won't work.
The end goal is to have 8+ analog outputs on the same digital bus, with all physically and electrically (except the i2c lines) isolated from each other. I would prefer to use i2c, but SPI is also an option. With i2c, most DACs only have 1 or 2 address select pins, supporting up to 4 devices. Is there a DAC that can support more addresses than this using i2c's 10-bit addressing scheme? Or is there a better way to do this?
Thanks for the advice.