hi all,
i am currently working with a sigma delta converter and i am in need of your help. the sigma delta converter is used for current sensing of a motor phase. The sigma delta converter's output is quite unclear to me. normally, it would be a 1-bit data stream. however, the datasheet mentions that the output from the modulator is unsigned 15 bits. I am using a HCPL-786J Sigma delta modulator. I found a way around this by choosing a HCPL-872; which, readily converts the output of 786j's output to 3-wire SPI output, ready to be interfaced with a microcontroller. MY question to you guys is..... Is there a way to directly interface this spi data to USB so that i can display the value of the measured current?? if so, how do i go about breaking down the data and (or) displayying it??? or you guys can give me a completely different approach without the HCPL-0872 chip.
What i know about the conversion from the Sigma delta modulator:
The current sensing from the modulator gives out 111111111111111 if the voltage across the shunt resistor is +320mV and 000000000000000 if -320mV where the first bit the sign bit.
P.S. I was also wondering if i could use TI's ZNP mini kit to read the output from the HCPL-0872 chip. Since, i am familiar with this development kit..... it would be great to know if i could just use the SPI to USB function of the kit and use a serial oscilloscope to represent the signal in analog domain.
Any help is appreciated.
Thanking you,
Nischal