Other Parts Discussed in Thread: ADS1015,
Hi team,
I replace ADS1015 in EVM with a ADS1013 because almost the same except some register and PGA setting. I replace U1 with ADS1013. But I have questions and issue below.
1. When I config it to single end mode AIN0-GND, and I apply a 1V voltage at AIN0-GND, the output voltage is not 1V. The output is not right. I find there is no mux for ADS1013. So can I drive ADS1013 by single end signal? Like AIN0=1V and AIN1=0V?
2 The EVM Userguide schematics is not the board's schematics now. It seems out of date. Could you share the latest schematics? There is no resistor between AINx and J1.
3 Where else do I need to pay attention for the replacement with ADS1013?
Best Regards
Michael