Other Parts Discussed in Thread: ISO7741
We plan to use daisy-chained modules populated by combination of the ADS8860 ADC and the ISO7741 isolator. We are dealing with communication timing and maximal SCLK frequency. Because of the isolators, the td-CK-DO = 13.4 ns MAX parameter (delay from SCLK going low to valid data on DOUT) mentioned in ADS8860 datasheet is important for our application.
I would like to ask, is there any relation of td-CK-DO time to SCLK frequency?
Second question is, how does td-CK-DO time relate to DOUT pin load (parasitic capacitance, etc.)? In our application, DOUT is connected to ISO7741 just through source termination resistor ~33 ohm.