I see where the scripts can be created. Is there a way to see the Machine Tx Rx hex code that the script generates for our uControl such as 55 40 08 55 42 08 55 48 48 ?
Peter
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I see where the scripts can be created. Is there a way to see the Machine Tx Rx hex code that the script generates for our uControl such as 55 40 08 55 42 08 55 48 48 ?
Peter
I tried the following commands and get no response. Any idea what is wrong? There is a .01sec delay after each hex number is sent. Commands are going into pin 16 on logic analyzer. Nothing on pin 15. Are any handshaking lines needed below?
55 06 55 40 00 55 41 00 55 42 00 55 43 00 send reset. set all config registers to 0
55 08 55 10 55 08 55 10 55 08 55 10 send start, RDATA, pause and wait for response but no response on ....
TX0 is transmit from uControl RX0 is uControl receive