I am using the ADC12D1X00RFRB reference board with Wave Vision 5 to evaluate a TI ADC. I am able to use the internal clock with a signal generator to look at an an input signal using the Wave Vision 5 software. According to the manual and the software options in Wave Vision 5, I am supposed to be able to input an external clock source to use with the ADC. I have tried selecting this option and using an additional signal generator to input a clock signal and examined the output from the ADC and do not seem to be getting good results (I am using a 1.8 GHz sine wave 0 dBm per the manual July 13, 2011 rev 1.0). Please advise on the proper way to configure the ADC12D1X00RFRB board to use an external clock source.
Thanks in advance for your time.
Mike.