Hi,
I'm using the TSW1400Board_CLib.dll to develop an application for the TSW1400EVM in combination with ads5282 to capture data triggered by an external signal (programming environment is Visual Studio 2010).
First of all after loading the Firmware into the board ("TSW1400BrdCtrl_Load_Firmware") the function returns an error_code of 20 which is not listed in the provided table TSW1400_Error_Codes.csv.
The main problem though, is that the external trigger mode appears not to work. I've set the variable "trigger" for "TSW1400BrdCtrl_Start_ADC_to_DDR" to 1 but the data is captured immediately without waiting for the triggering signal (triggered by pushbutton). If I use that same signal with the HSDCP the triggering option works fine.
Can anybody give me some information how the trigger option whithin a software application should be implemented?
Thanks.
Regards,
Kathrina