Hi all. I am using a TSW1400EVM pattern generator for a high speed characterisation system, which I would like to control via Labview. I see that the GUI's shipped with the module are Labview based, and there are a number of example VI's for firmware and waveform download supplied with the GUI software. However, when I try to open these VI's Labview finds that there are pieces missing. For example, "TSW1400.lvlib:TSW 1400_Token compatibility for C.vi" (for Firmware_Download.vi)
I've searched for this lvlib file on my entire C drive, and it doesn't exist. Can anyone suggest how I find these files? Also, when I open 1400_DAC_Write.vi, some of the call library interface nodes have no path set up, whilst others have paths hardcoded to someone elses install. The latter case I can figure out how to correct, but the empty ones I haven't managed to guess since there is no dll name to search for.
Many thanks for any suggestions.
Robin Wesson