Hello,
I am trying to use the SYNCOUT (pins F2, F1, P5, N5) signal of the ADS5409 converter, but have trouble with it. I run the ADC with a CLKIN at 500 MHz and I would like to use the SYNC feature to synchronize 2 ADS5409. The SYNC input (P9,N9) is fed with a 15.625 MHz LVDS signal, which is derived from the sampling clock divided by 32. According to the data sheet REVA p.25 (January 2014), I should get also a 15.625 MHz on the SYNCOUT pins. But what I get is a LVDS signal which toggle every 2 ns, and the pattern is dependent of my analog input sine wave. All happens as if the SYNCOUT pin is like a data bit!
Do you have an explanation of this unexpected behavior?
Thanks,