What is the lowest frequency of conversion that this ADC can perform?
How close to DC or 0 Hz can it perform conversion?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the lowest frequency of conversion that this ADC can perform?
How close to DC or 0 Hz can it perform conversion?
Hi John,
There is no lower frequency limit as long as the driving interface is DC coupled. For instance, a fully differential amplifier could be used in a DC coupled arrangement to drive the ADC. Note that our EVMs usually have transformers on the input which will not block DC. In this case, the transformer will limit the lower input frequency of the EVM.
Regards,
Matt Guibord