Hi
I am looking for the vhdl/verilog code of the TSW1200, can you send me a copy? My email is jothiadithya@gmail.com
Jothi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I am looking for the vhdl/verilog code of the TSW1200, can you send me a copy? My email is jothiadithya@gmail.com
Jothi
Hi,
There are two separate sets of Verilog code for the TSW1200 so I need to know which one you need. The eeprom on the TSW1200 is large enough to hold two bit files. There is a bit file for parallel LVDS DDR data busses such as would be used for a device like ADS4149 for example, and there is a bit file for serialized data busses such as would be used for ADS5281 for example.
What would be the part number of the ADC that you would be using so that I could tell if you want the code for the parallel DDR format or the serialized fornat?
Regards,
Richard P.
Hi,
I would like to interface with AFE5805EVM. I would need deserializer vhdl/verilog code. Please send to jothiadithya@gmail.com
Jothi
Hi,
This code is having PMCD of virtex. I am using zynq (7 series), how do I replace this?
jothi
Hi,
You'll have to go to Xilinx for support on the usage of specific Xilinx products or Xilinx cells. That is what we would have to do if we were to try to port this code to a newer platform like Zynq.
Regards,
Richard P.