Hi,
The ADC1175 has a dynamic capacitive load (4pF when the clock is low and 11pF when the clock is high). Is this why there is a 62pF capacitor in the reference circuit on page 16 on the datasheet? Can I get away without a capacitor there?
I only need a GBW of about 10MHz. I am having trouble determining a general purpose OpAmp that can adequately drive the dynamic capacitance. Can I use general purpose OpAmp like the LMV796?
On the bottom reference (VRB) the datasheet shows a 1N4148 diode. I would assume I should remove this since I will be setting VRB to 1.8V
Also, when generating reference voltages (pg. 18), it is suggested that 10uF tantalum caps are used. What are the drawbacks of using ceramic or electrolytic?
Thanks,
Eric