Hi. I have DAC3484EVM plugged into TSW1400. My goal is to use it as an arbirary function generator to create two pulse waveforms with amplitude of 2Volts at 1700 Hz with pulse duration of 2 us. The pulses are ON for 2 us then OFF by 588 us. Channel #1 and Channel #2 needs to be delayed from each other by 100 us. Also, I would like to create various files with different rise rise times use onboard clock (CDCE62005)?
Q1- When I am creating a .csv file, should I use 32,768 data points for one period of the pulse waveform ( 32,768 points is used for 588 us duration)
Q2- What should I put for Data Rate (SPS) for generating 1700 Hz pulses?
Q3- When I load a file from the \Test Files folder like '"single_tone_cmplx_32768_250MSP_BW_25.1MHZ.csv" for understanding how this board generate a signal, I see thast I enter 250 SPS and fft graph below shows the 25 MHz frequency. Can anyone explian to me the connection between 250SPS input and 25 MHz fft frequency? the fft frequency is always 10 time smaller than SPS input??
Q4- Do I need to modify my board to by pass the EVM board ADT4-WT balun which has a 2MHz lower bandwidth?
Q5- When I load my 32,768 data point for generating my 2 us pulses I see lots of harmonics? Is this normal?
I appreciate answers to my questions.
Thanks
Joseph