Hi,
i have two questions about DAC908.
1. - What it the output compliance voltage when operating at 3V power? I could only find that it is 1.25V using 5V power.
2 - Can VD and VA power input pins be different voltages? I have digital Inputs that are 3.3V, but would like to operate the VA at 5V to get best output voltage compliance. If that is not possible, then I really need to know the output votlage compliance for 3V power.