I have questions about the DAC5688.
I using the DAC5688 chip as a DUC(Digital Up Converter).
DAC5688 input data are I, Q values. (IQ sampling)
And I using FMIX(Full Mixer) and NCO.
Question1) When the DAC input clock is 320 MHz (under external clock mode), maximum NCO frequency is limited up to (320/2) = 160 MHz ??
I want to generate the DAC output signal frequency of 200 MHz. If can, please advise me how to rising the DAC output signal frequency up to 200 MHz.
Question2) DAC5688 input data(I, Q values) rate is influencing to the DAC output signal frequency?
I hope your advice and warm answer.
Thank you very much ~!
Thanks.
Mr. Jeongslaa523a.pdf