We are using the DAC37J82 on a custom card. I’m going thru its datasheet, and have several questions regarding its register settings. I've tried using both the DAC3XJ8X and TSW3XJ8X software, but they don't offer much insight for some of the register settings.
Our application is summarized as follows:
- 240MHz DACCLKp,n ref clk input
- using the onboard DAC PLL configured to 4320MHz, P=3, M=6, N=1
- DAC output rate = 1440MHz
- with SERDES PLL = 1800MHz using the PLL (DAC) clock as input (MPY = 5, REFCLK_DIV=4).
- We have a several bandwidth, lane variations we’re considering, and will configure their L-M-F-S-HD and RATE accordingly.
a) 2-lane, 180MHz input data rate, interpolation = 8, 3600Mbps SERDES line rate -- configured as 2-2-2-1-0 and half RATE
b) 4-lane, 180MHz input data rate, interpolation = 8, 1800Mbps SERDES line rate -- configured as 4-2-1-1-1 and quarter RATE
c) 4-lane, 720MHz input data rate, interpolation = 2, 7200Mbps SERDES line rate -- configured as 4-2-1-1-1 and Full RATE
- What LB setting is recommended for SERDES VCO clk of 1800MHz using DAC clk (1440MHz) has it’s input reference?
- What should the clkjesd_div setting be? It's used for JESD clock, but datasheet doesn't mention what rate it should be.
- How do we determine the pll_vcoitune and pll_cp_adj settings?
- Some of the registers are labeled with ‘FUSE controlled’. Do these registers require any special consideration?
Thanks.