Hello t
Hello there,
I have a question regarding DAC38J84 Evaluation Module.
In fact, in this board DACs outputs are connected through the RF transformer in order to get the single end output signal. My problem is that together with RF signal, I need to generate the all-positive baseband signal with frequency range from DC to 100 MHz. For this purpose I am going to use one of DACs placed in DAC38J84 evaluation board. The problem is that the RF transformer in the evaluation board has pass-band from 50 MHz. My question is: are there some possibilities to generate all positive signals at low frequencies starting from DC and what modifications are required for DAC output circuits? Thank you for support.
Alex
here