Hi,
Let me ask you a question with the LINK status of DAC3xJ84.
Data sheet(SLASE17B) page96
bit1 = read_error : Asserted if read request with empty FIFO
bit0 = read_empty : FIFO is empty
Q1.
Please explain the meaning of bit0 and bit1 (difference between both).
As a result of confirmation by evaluation, bit0="0" and bit="1" are set.
When FIFO is in empty state, it is thought that bit1="1" because read was executed,
If FIFO is in empty state, we think that bit0="1".
However, bit0="0" and bit1="1" are confirmed.
We think that bit0="1" and bit1="1" when FIFO is empty, is it wrong?
Q2.
bit1 = read_error : Asserted if read request with empty FIFO
In which phase of the JESD204B interface is the phase in which bit1 error occurs?
Is it code group synchronization (CGS), or initial lane synchronization (ILAS),
or will it occur in the data transmission phase?
best regards